web counter

Cryogenic Cooling Technology using SiC and GaN Devices

Published: 07 July 2023 | Last Updated: 07 July 20232905
Hello everyone, welcome to the new post today. This article introduces the characteristics and challenges of WBG devices in cryogenic cooling applications and demonstrates their operation.
Topics covered in this article:
Ⅰ. Demonstration of SiC Converters Using Cryogenic Cooling
Ⅱ. Demonstration of MW-level sic converter operation with cryogenic cooling
Ⅲ. Challenges SiC and GaN in cryogenic cooling Applications
Ⅳ. Conclusion

Even though power electronics have made significant advancements utilizing established silicon (Si) devices, the focus is now shifting towards Wide Bandgap (WBG) semiconductor devices, specifically Silicon Carbide (SiC) and Gallium Nitride (GaN). These WBG devices have garnered increasing attention due to their notable characteristics, including low on-state resistance, high-speed switching, and high breakdown voltage. Power converters based on WBG semiconductors exhibit significantly enhanced performance, efficiency, power density, and reliability compared to converters employing traditional Si devices.

The application of cryogenic cooling, which involves ultra-low temperatures below 123 K, shows future scope in power electronics. Cryogenic cooling is typically achieved through the utilization of substances like liquid nitrogen or helium and offers numerous benefits for power electronics. Integrating power electronics into cryogenically cooled systems eliminates the need for separate thermal insulation containers, thereby reducing complexity, cost, size, and weight.

Cryogenic cooling holds significant potential for various applications, including electric aircraft propulsion systems or superconducting machine systems, where the integration of power electronics within the cryogenically cooled environment can substantially enhance system performance and reduce overall complexity. Furthermore, cryogenic cooling can offer general advantages for power electronics, such as improved performance of WBG semiconductor devices at low temperatures, the ability to operate devices at higher switching frequencies, reduced cooling requirements, and the potential for lightweight and efficient conductors.


Ⅰ. Demonstration of SiC Converters Using Cryogenic Cooling

 Device characterization at cryogenic temperatures:

To examine the behavior of power devices under extremely low temperatures, a cryogenic temperature chamber is commonly used in laboratory settings. This chamber utilizes liquid nitrogen to regulate the temperature, allowing it to range from room temperature down to a minimum of 93 K. The chamber is designed with thermal insulation both inside and outside to maintain the desired temperature.

 Figure 1 Test setup for demonstration at cryogenic temperatures..png

Figure 1: Test setup for demonstration at cryogenic temperatures.

A setup similar to the one shown in Figure 1 is used for static characterisation tests. The B1505A curve tracer is connected to the Device Under Test (DUT) to measure its output and transfer characteristics. A Kelvin connection technique is employed to minimize measurement errors caused by long cables.

Summary of SiC and GaN devices characteristics at cryogenic temperatures

Figure 2 illustrates a comparison of the specific on-state resistance of the selected devices. Both silicon (Si) MOSFETs and gallium nitride (GaN) HEMTs exhibit significantly lower specific on-state resistance at cryogenic temperatures. However, Si MOSFETs start to experience an increase in specific on-state resistance at very low temperatures (< 100 K) due to carrier freeze-out, while GaN HEMTs continue to decrease in resistance.

Figure 2 Specific on-state resistance versus temperature between different devices..png

Figure 2: Specific on-state resistance versus temperature between different devices.

All-silicon carbide (SiC) MOSFETs on the other hand demonstrate a notable increase in specific on-state resistance at cryogenic temperatures. Among the devices, GaN HEMTs exhibit the lowest specific on-state resistance at cryogenic temperatures, achieving more than a fivefold reduction compared to room temperature values.

Figure 3 Breakdown voltage versus temperature for different devices..png

Figure 3: Breakdown voltage versus temperature for different devices.

 As shown in Figure 3, SiC MOSFETs and GaN HEMTs generally exhibit relatively constant breakdown voltages, while Si MOSFETs display reduced breakdown voltage as temperature decreases from room temperature to cryogenic levels.

 

Ⅱ. Demonstration of MW-level sic converter operation with cryogenic cooling

A high-power silicon carbide (SiC) power module-based inverter designed for electric aircraft propulsion applications can deliver a megawatt (MW) of power. This inverter utilizes cryogenic cooling technology to enhance its performance. It operates with a DC input fed from a ±500 V bus to eventually generate a three-phase output with a fundamental frequency that can reach up to 3 kHz.

Device selection

Si MOSFET and GaN HEMT devices excel at cryogenic temperatures, but the lack of high current power modules and suitable commercial packaging poses challenges for an MW inverter. Consequently, a high-current SiC power module is chosen. Although direct cryogenic cooling is not feasible for SiC, cryogenic temperatures still benefit the inverter by providing a lower ambient temperature environment, resulting in lower SiC device junction temperatures during high power operation and improved efficiency. Cryogenic cooling also benefits busbars and filter windings.

Characterization is limited to temperatures above 225 K to protect the silicone gel. The lowest on-state resistance is achieved around 257 K, optimizing the cooling system to maintain the junction temperature near this value. The inverter uses a three-level active neutral point clamped (3L-ANPC) topology, with two 500 kW inverters paralleled and interleaved through coupled inductors to achieve 1 MW power output while reducing harmonic ripples. EMI filters suppress noise and meet DO-160 standards for aircraft applications.

Cooling system design and integration

Figure 4 Cold gas nitrogen cooling concept..png

Figure 4: Cold gas nitrogen cooling concept.

 To overcome the limitations of direct liquid nitrogen cooling for the SiC power module, an alternative approach utilizing cold nitrogen gas cooling is adopted. Figure 4  illustrates the cooling concept, where nitrogen gas passes through coils submerged in a liquid nitrogen bucket. The gas is cooled by the liquid nitrogen and then directed to a cold plate for the power module. The cooling performance can be adjusted by controlling the flow rate of the gas through a regulator and adjusting the number of coils turns submerged in liquid nitrogen.

 

Ⅲ. Challenges SiC and GaN in cryogenic cooling Applications

Cryogenic cooling offers improved performance for wide-bandgap (WBG) devices, particularly GaN HEMTs, compared to room-temperature cooling. It also provides benefits to WBG-based power converters, such as reduced cooling requirements due to the lower operating temperature and the utilization of lightweight and efficient conductors (e.g., busbars and inductor windings) at low temperatures. Nonetheless, implementing cryogenic cooling in power converter designs poses new challenges that require careful consideration. The application of WBG devices with cryogenic cooling is still in its early stages and has yet to reach technology maturity.

Packaging

Packaging power modules involves electrical, thermal, and mechanical design considerations. Researchers and manufacturers are addressing the need for packaging technologies that minimise parasitics, achieve current and thermal balancing among multiple dies, and withstand high electric fields and temperatures. But, commercially available packages do not account for cryogenic operation.

Silicone gel-based encapsulants commonly used in packaging are unsuitable for cryogenic temperatures due to reduced breakdown voltage caused by the partial discharge. Epoxy-based materials can function at cryogenic temperatures, but brittleness is a concern. Packaging without encapsulation is an option, but it may expose modules to environmental damage and compromise insulation. Thermal-mechanical stress is another challenge, necessitating careful management of thermal expansion coefficients to prevent packaging degradation and device failure.

EMI filter

The EMI filter plays a crucial role in suppressing EMI noise and meeting EMI standards in power converters. Cryogenic temperatures enable faster switching, allowing for higher operating frequencies and reducing the need for passive EMI filters. However, this also concentrates EMI noise in the high-frequency range, making filter design more challenging due to the non-ideal behaviors of passive components and coupling effects. Cryogenic cooling benefits the inductor winding but negatively impacts the magnetic core. Optimizing filter housing design to balance core and winding losses and maximize cryogenic cooling benefits requires further research.

Cooling system

Cryogenic cooling systems pose greater complexity and challenges compared to room-temperature cooling systems. Specific requirements for cryogenic cooling include factors like ensuring no leakage to prevent high-pressure buildup within the converter enclosure due to the significantly higher density of liquid nitrogen compared to air. Hence, providing adequate thermal insulation to protect operators from the extremely low temperatures of liquid nitrogen and preventing injury and ensuring good air insulation as the low temperature of liquid nitrogen or cold gas can cause vapour in the air to freeze and potentially lead to short circuits within the converter. Safety considerations and risk assessments should be incorporated into the design of the cooling system.


Ⅳ. Conclusion

GaN HEMTs significantly reduce on-state resistance at cryogenic temperatures, while SiC MOSFETs show increased on-state resistance. GaN HEMTs demonstrate faster switching speed and reduced switching loss, while SiC MOSFETs exhibit slower switching speed and increased switching loss at cryogenic temperatures. Both types of devices maintain relatively constant breakdown voltages across a wide temperature range.

A cryogenically cooled MW-level SiC inverter achieves high power operation and efficiency, making it a promising solution for aircraft propulsion. High-current operation of GaN HEMTs with cryogenic cooling is also demonstrated. Challenges and considerations for packaging, gate drive, protection, EMI filtering, and cooling systems are discussed, emphasizing their importance in cryogenic cooling applications for WBG devices.


Saumitra Jagdale

Saumitra Jagdale is a Backend Developer, Freelance Technical Author, Global AI Ambassador (SwissCognitive), Open-source Contributor in Python projects, Leader of Tensorflow Community India, and Passionate AI/ML Enthusiast

Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242928

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255726

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20262139

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261128

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026981

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More